Other Parts Discussed in Thread: LMX2485, LMX2491, LMX2492
I have a customer with IBM who is asking the following questions regarding the LMX2594:
I am trying to make a classical linear 800MHz-1GHz FMCW waveform (triangular in the frequency domain) without any stops. Tried dozens of configurations and was not able to make one of them work. Since that your design incorporates few VCOs, I decided to choose VCO4 that has the widest bandwidth (10.8-12GHz). The only option that make it work was to lock and start at 10.9GHz and to set a short time for the ramp. Please advise what is the widest FMCW ramp possible with this chip?
Can he do this with the LMX2594? Does he need use a different chip? Different configuration?
Thanks for your help with this!
Richard Elmquist