Dears,
The customer is using LMX2594, now he have some problems.
When using the manual ramping example (Datasheet Page 27) . The signal will suddenly lose lock in the process of manual ramping. The start frequency is 10GHz, and the step forward is 10MHz, at about 10.130GHz the loss of lock will occur, after about 30s the signal jump to 10.450GHz, then the signal will return to normal.
RAMP_TRIG_CAL=0, RAMP_THRESH=300MHz, because the customer said when set RAMP_TRIG_CAL=1, the ramping do not work.
I want to know how to solve this problem.
Regards,
Ricardo