Hello! The datasheet is not clear on what has to be done with the following pins if unused:
SYNC
SysRefReq
RampClk
RampDir
RFOUTBP
RFOUTBM
Can all of them be left open?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello! The datasheet is not clear on what has to be done with the following pins if unused:
SYNC
SysRefReq
RampClk
RampDir
RFOUTBP
RFOUTBM
Can all of them be left open?
Thanks.
Mikhail,
Yes all can be left open.
For RFoutBP/BM, you definitely want to leave these open as they are outputs.
For SYNC and SysREFReq, you could ground them, but if you set INPIN_IGNORE=1, they are ignored.
For RampCLK and RampDIR, they do nothing if RAMP_EN=0.
So in summary, you could leave all these open and should definitely leave the RfoutBP/BM open.
You could ground SYNC,SysRefReq, RampCLK and RampDir if you want to, but it is not necessary.
Regards,
Dean