This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2492EVM: Resistor R12 for RFout/4

Part Number: LMX2492EVM

Hi All,

Please could anyone advise as to whether one should populate resistor R12 if RFout/4 is going to be used?

I want to use RFout/4 in a 50 ohm system and R12 seems to be needed for a 50 ohm tee network? The board is however shipped without it.

I assume the output impedance of the RFVC1843 is 100 ohm (from Fo/4), which would correspond to the chosen values for resistors R11 (18 ohm), R12 (68 ohm) and R13 (18 ohm)?

If these assumptions are correct, do we expect a 10 dB drop in output power? The power out of RFout/4 would then be approx -12 dBm?

Please let me know if I'm completely off the mark?

Kind Regards

Darryn Jordan