This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03328: Jitter performance differences between CLKOUTx clocks and STATUSx clocks.

Part Number: LMK03328

Hi Team,

Please advise me on the jitter performance differences between CLKOUTx clocks and STATUSx clocks.

I want to use 30 MHz 3.3V LVCMOS clocks from LMK03328, (REF = 30 MHz)


The CLKOUTx does not support 3.3V LVCMOS output. So, level sifter ICs may be used with
LMK03328, when CLKOUTxs are used,


In the meantime, LMK03328 can output 30 MHz 3.3V LVCMOS clocks through STATUSx pins.
I want to know jitter performance difference between these two cases.


Please also let me know if there are any restrictions on functionality when STATUSx output is used compared to
The case CLKOUTx is used.

I appreciate your prompt feedback, because I want to fix design before the end of this week.

Mita