Hi all,
can you please let me know what is the voltage on the CPOUT (PIN 12) & VREGIN(PIN 10) OF LMX2594
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
can you please let me know what is the voltage on the CPOUT (PIN 12) & VREGIN(PIN 10) OF LMX2594
We don't have current numbers for the individual pins
I need to look into this
thanks it will also be helpful if you can give the internally generated voltages on pins 36,29,38,33,3,27
Thanks for the reply Dean.
are you referring to pin 37 as VCC_PLL or both pin 37 & pin 26 combined as VCC_PLL. I am unable to find VCC_PLL in the pn functions table.
Also which series resistors are you referring to ? can you please confirm the block diagram no. ?
Please can you also let me know what is the i/o standard type. It appears to be PECL /CML sort of something ?
Siddharth,
The outputs are open collector and are pulled to Vcc. The output voltage varies with Vcc, OUTA_PWR setting, and frequency and is expressed in dBm for some of the typical performance charts. At higher frequencies, this resembles a sine wave, but closer to a square wave at lower frequencies.
There is no Vcc Pin. There is VccDIG, VccMASH, and VccCP. I would expect VccCP and VccDIG to have higher current.
As for the series resistors, note that there are not any in the typical application schematic on section 8.2. It recommends shorting the supplies together and this is why we don't have individual current numbers per pins. On our EVM instructions, figure 12, we do show series resistors, but they are all 0 ohm. I thought this was what was prompting your questions.
Regards,
Dean
thanks Dean. I was trying to understand your previous reply on current draw. So at no load the current draw will be 248ma right? is this no. certain or is there any doubt in this as well?
Also it appears from your reply that its not certain how the no load 248ma is appearing? because the constituent supplies VCC_MASH, VCC_DIG don't consume more than 10ma as per you. Am i correct?
Siddharth,
"no load" is to vague. I mean OUTA_PD = OUTB_PD = 1. The 248 mA is fairly predictable, but it does vary based on setup conditions charge pump, phase detector). Remember in this state, the PLL and VCO are still both powered up and running. A lot of the current will be going through VccVCO/VccVCO2, then next could be VccCP. The PLL current can be divided amoung several pins.
What is prompting all these questions about current per pin? The supplies are shorted on our EVM.
Regards,
Dean