This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Output Power Control with OUTA_PWR / OUTB_PWR

Part Number: LMX2594

The Datasheet is LMX2594 tells that R44 [13 : 8] controls the OUTA_PWR  and similarly the R45 [5 : 0] controls the OUTB_PWR.

For a 50 Ohm resistively coupled output, what is the Minimum and Maximum Power output of the device ? Basically I wish to know the effect of the 5 bit control on the output power.

  • Dear Jayant,

    The output power range witht he 50 ohm pull up configuration is approximatly 10 dB. Having said that, this output is NOT a calibrated output and will have a diffrent response with respect to operating frequency.

    I hope this helps.

    Regards, Simon.