This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ADC12DJ3200: JMODE16 Link Alarm

Prodigy 70 points

Replies: 6

Views: 258

Part Number: ADC12DJ3200

I am attempting to use JMODE 16 with Fs=1000MHz. I have confirmed that KM1 and Octets per frame match the other side of the link.

After initialization, I read JESD_STATUS and ALM_STATUS and get these values:

JESD_STATUS (0x208) -> -0x1c (REALIGNED, ALIGNED, PLL_LOCKED)

ALM_STATUS (0x2C1) -> 0x8 (Link Alarm).

There have been times when I have read 0x7c out of JESD_STATUS, but then soon after I read 0x1c. 

Sometimes when I clear the REALIGNED bit of JESD_STATUS, it doesn't come back for a while.

The largest spurs in my clock source are about 50 dB down a few kHz away from the main lobe. I have not ever observed Clock Alarm in the ADC.

Any thoughts on what would cause the link to behave this way?

Thanks,

Cam

  • Hi Cam
    What K or KM1 value are you using?
    Do you have SYSREF receiver and processing enabled or disabled?
    If they are enabled what is the frequency of SYSREF you are applying? Do you have a continuous SYSREF?
    If they are enabled can you try disabling SYSREF processing to see if that changes the results you are getting?
    Best regards,
    Jim B
  • In reply to Jim Brinkhurst84999:

    Hi Jim, thanks for the reply.
    I am currently using KM1 = 0x1F.
    Are you referring to SYSREF calibration? I don't have that enabled. Register 0x2B0 -> 0x0 at the moment.
    My SYSREF frequency is a continuous sine wave at 1.953125 MHz. Is that the correct frequency for sampling 1000 MHz?

    Thanks,
    Cam

  • In reply to Cameron Grant14:

    Hi Cameron

    For KM1 = 1Fh (K Minus 1 = 31d, K = 32d) and Fclk = 1000 MHz the applied SYSREF should be 1.953125 MHz or a sub-harmonic of that frequency. 

    Please ensure that is the frequency being applied at the ADC SYSREF input. SYSREF must be frequency and phase locked with the ADC CLK signal.

    If the frequency is correct and the errors are still happening try disabling SYSREF processing to see if that changes anything.

    Set Register 0x029 = 30h (SYSREF_PROC_EN = 0). 

    If that eliminate the link alarms you are getting then you probably need to use SYSREF Calibration to optimize the setup/hold time between CLK and SYSREF. Please refer to Automatic SYSREF Calibration in the ADC12DJ3200 datasheet to see the steps required.

    Best regards,

    Jim B

  • In reply to Cameron Grant14:

    Hi, 

    Does the JESD204B tx state machine in the ADC look like the one in the JEDEC standard? The diagram from the standard (below) makes it look like the only two things that could kick the tx machine out of DATA_ENC are sync_request_tx and reset. I can see now that the sync signal from my receiver is toggling at a frequency that looks similar to the SYSREF frequency. I imagine that is why I am receiving this alarm? Why would my receiver be struggling to get code-group synchronization?

    Do you happen to have a JMODE16 example design that uses Xilinx JESD204B cores?

    Thanks,
    Cam

  • In reply to Jim Brinkhurst84999:

    Hi Jim,

    I will try the SYSREF_PROC_EN=0 and get back to you.

    Thanks,
    Cam
  • In reply to Cameron Grant14:

    Hi Cam
    Sounds good, let me know how that goes.
    One additional point on SYSREF for this ADC. If you have an application that doesn't need deterministic latency or synchronization of data between multiple converters you can leave the ADC SYSREF processing and SYSREF receiver disabled permanently and turn off the ADC SYSREF signal from the clock chip. The ADC internal LMFC timing self starts without SYSREF and everything operates normally.
    Best regards,
    Jim B

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.