• TI Thinks Resolved

ADC128D818: When ADC128D818 internal Temp is used , One ch need to compromised?

Prodigy 310 points

Replies: 1

Views: 35

Part Number: ADC128D818

In  ADC128D818 internal  temp. sensor available excluding the 8 input channels of ADC? If not, which channel is compromised to get temperature details?

  • Hi Dilip,

    If you review the operating modes of the ADC128D818 in section 8.6.x of the datasheet, you will see that you can use CH0-6 and temp in Mode 0 or CH0-7 in Mode 1.  In modes 2 and 3 you can use all channels (in various pseudo-differential configurations) plus temperature.

     

    Regards,

    Tom