This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPL0102-100: TPL0102-100

Prodigy 30 points

Replies: 5

Views: 101

Part Number: TPL0102-100

Hello.

1.regarding tolerance of 20% end to end.

   does the table list of all the resistance in page 15 are reliable?

2. BIT ASSIGNMENT : BIT 7= VOL, BIT 6=SHDN, BIT 5= WIP .

   Does BIT 0,1,2,3,4,5 are register address?

thanks Kobi.

  • Hi Kobi,

    1. The total resistance can vary ±20%, but the linearity is still ±0.5LSB.  So that values in the table could vary ±20% as well, but they would all vary nearly the same amount.  So for example, in the worst case, all values would be +20% larger, but it is not possible for one value to be +20% and the next to -20%.

    2. The ACR is its own register, with the address of 0x10.  Bits 0-4 are "don't-care" or reserved bits. 

    Thanks,

    Paul

  • In reply to Paul_Frost:

    thanks.

    1. that could be a problem for my design since it base on a static resistance in power up.

    do you have other component that have 1% tolerance in total resistance?

    2. according to your answer, after ACR configuration I need to send another 8 bits of op code.

    Kobi. 

  • In reply to kobi cohen1:

    Hi Kobi,

    Could you give a little more detail about your application? Maybe a precision DAC could solve this.

    In regards to the ACR register - this register is just like any other.  It can be read and written to using the same methods as described in section 7.5.2 of the PDS.

  • In reply to Paul_Frost:

    Hi

    the project is accurate dynamic power regulator from 0.6V-5V.

    The Board will have 8 power circuit like that can be adjustable.

    so I need to have stable known resistors that I can change and control via micro controller.

    thanks Kobi.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.