• TI Thinks Resolved

Compiler/TSW1400EVM: SDK/API

Prodigy 80 points

Replies: 3

Views: 81

Part Number: TSW1400EVM

Tool/software: TI C/C++ Compiler

Hi --

I was wondering if there is a Software Development Kit (SDK) available for the TSW1400EVM. Do you have any programming examples that you could share?

How about a Application Programming Interface (API)?

Best,

Yamuna

  • Guru 51130 points

    Yamuna,

    There is no SDK. If you install the HSDC Pro GUI software, you can find examples under the HSDCPro Automation DLL and Automation Functions APIs directories shown below.

    Regards,

    Jim

  • In reply to jim s:

    Thanks Jim. Did you mean to share the examples? Also are there any examples that you can share where I could import the data into a Visual studio interface say? 

  • Guru 51130 points

    In reply to Yamuna Phal:

    Yamuna,

    Here was the reply from our software team regarding your question:

    The existing Automation DLL has APIs to export data from HSDC Pro (as a .csv or .bin file), which can be imported in any programming language for further processing. Kindly refer to “HSDCPro Automation DLL Manual.doc” (available at the following location) for more information about the functions and their definitions exposed in Automation DLL.

     

    HSDCPro Automation DLL Manual Location : “[HSDC Pro Installed location]\HSDCPro Automation DLL\Manual and Examples\HSDCPro Automation DLL Manual.doc”

     

    Default HSDC Pro Install location : “C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro”

    Regards,

    Jim