Hi,
I successfully managed to read voltage from an PT100 sensor, now I am trying to use the system monitor in order to make a system check. I thought the sequence to do so is as follow:
1-Configure MUX1 register to select a system monitor (write to MUXCAL2:0, 0x03 for temperature diode)
2-Send RDATA command
3-Send 3 NOP commands and read Datas
I tried to get measurement this way but I didn't receive a good result (118mv for 25°C, so I should get a close value).
Is there something missing in this operation?