ADS1278, Settling Time. The datasheet specifies Settling time for 3 modes: High Speed, Low Power and High Resolution, but it does not even mention "Low Speed" Mode setling time. Could you please provide this information ? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS1278, Settling Time. The datasheet specifies Settling time for 3 modes: High Speed, Low Power and High Resolution, but it does not even mention "Low Speed" Mode setling time. Could you please provide this information ? Thanks
Thanks Greg, yes, I did find it there.
Just to make sure I understand the definition of "Settling time": this would be the time it takes to settle after an input step,right ? Does it depend on the step amplitude?
For instance: Clock at 1MHz, Low Speed Mode, that gives me a fDATA of 390.625Hz (1Mhz/2560). Input: step from 0V to 5V, will it take 194.56 msec to settle in Low Speed Mode (76/390.625) ? What if the step is 0.5V ?
Thanks again
Matias Brusco