Hello,
I would like to ask about the single ended input range of the ADS131E08S, if I use a unipolar power supply of Avdd=5V and use the internal Vref=2.4V, and set INN=0 V, what is the allowed voltage range at the INP? can it varry varry between -0.3V and 2.4V? taking in to consideration the limit imposed by the Avdd?
What if I use a bibolar power supplu -2.5 to 2.5 V, and use the internal Vref=4V, set INN=0V, Is the allowed voltage range at the INP varry between -2.8V and 2.1V? taking in to consideration the limit imposed by the Avdd?