Hello
i have bought the AFE4300 because it support 4 load cells for a weight scale measuring using a cheap Ebay Sensors (4 Pieces) with 3 end Cable black white and Red i think its a half bridge im not sure the Project its from the School and i need to do it i don't have a lot of Time the Idea of the Project is to build a body scale system so all of the 4 sensors musst give a summ of the voltage to the AFE4300 Module and be converted in binary and take the Result and show it with a Microcontroller Cortex M3 and sho it on the LCD for example 15 kg musst be shown on the Display the problems now i have now idea how to connect all the Weight Sensors to the AFE4300 i have read the manual and i still have no idea even the Professor don't know exactly where we can put all of the wires every load cell have 3 wires also 2 resistor that means 4*3 = 12 wires for the 4 load Cell i really need your help i Schema or something how i can connect all the 4 Sensors to the AFE4300 Analog front end converter here are the sensors :
please write in Ebay : 4pcs 50Kg Body Load Cell Weighing Sensor Resistance strain Half-bridge Total.
and you will find the Sensors what im talking about i need tu use 4 of them also connect all the 4 with AFE4300 Module i did found nothing in the user manual and on the internet so please help me and im waiting of your reply i can explain again everything what i mean and thanks