Device ADC16DX370RMET need US re-export license required?
If the parameters shown below are met or exceeded for the part ADC16DX370RMET with US ECCN 3A001. a. 5. A
if US re-export license is required pls support written/email confirmation)
For ECCN3A001. a. 5. a
1) Pls get manufacturer/Supplier written / e-Mail confirmation on the part ADC16DX370RMET, if it is
1) "designed or modified" for military use,
2) Hermetically sealed and
3) Rated for operation in the temperature range from below -54 Degree Celsius to above +125 Degree Celsius
Now customer will be tested in the chamber with target system for device environments test, the chamber temperature can be changed -40 to 85 (some case 100 degree) with humidity, but target is guarantee up to 85 degree operation