Hello,
I'have design a board with the ADS8598H following this application note to increase the input range to +-25V : http://www.ti.com/lit/an/sbaa244/sbaa244.pdf, but I have a problems with this note:
According to the note, I chose 2 resistors of 1.5Mohm so :
Vin = Vinadc.(Rin+Rext)/Rin = 10*(1.5+1)/1 = 25V
But at 12.5V the output code become negative so the practical range is +-12.5V and I don't understand why.
Moreover, when I compute the input voltage with this equation:
Voutadc = code * 2 * FSR / (2^n)
I have a factor two compare of the real equation.
Is the an problem with this note or I done something wrong ?
Thank you