Hello,
I'm trying to make ADS1220 work. I'm using a PSOC to communicate with SPI. The SPI signals from the PSOC is correct. However, I'm not quite sure what to expect from the ADC, as I'm not sure if I have set it up correctly. I haven't added any reference as I understand that it's using it's internal reference voltage by default. Shouldn't the ADC output a value even though there's nothing on the inputs?( in that case it should send 24*0, but the output pin is constantly high.
Also, when I measure REFP0, it's connected to ground, while having REFN0 as VDD. Isn't this opposite?
Any advice is appreciated, and I have attached a link to current simple setup.
DVDD, AVDD and SPI voltage is all 5 V.