Other Parts Discussed in Thread: ADC12DJ3200, LMK04828, LMX2582, TSW14J57EVM
Hi,
I have successfully connected ADC12DJ3200EVM with TSW14J57 (Rev E) and have been able to sample a signal with JMODE0 setting. I have mod-ed the board to use external clock source.
ADC Clock - 1966.08 MHz (connected to DEVCLK and LMK_CLKIN
Signal - CW @ 491.52 MHz
Now i am trying to use JMODE3 and i am not able to sample my signal. I want to sample an I/Q signal (I Connected to VINA and Q connected to VINB)
See ADC12DJ3200 GUI Screenshot below. Seems to program the ADC without problems.
The HSDC4.9 Capture is as follows
However for some reason the "RX CLK" LED D4 is just high and not blinking. When I try to capture data, i get the following error
I am not sure what I am doing wrong. JMODE0 worked without any problem.
Sai.