Part Number: TSW1400EVM
hi TI~
I am having trouble with the TSW1400EVM+ADC3484EVM, please provide help, thank you!
Question 1:
When using the TSW1400EVM+DAC3484EVM,I uses the data file from the HSDC Pro(\Texas Instruments\High Speed Data Converter Pro\Test Files\xxx.tsw) to test. It's OK.
However, after the data collected by our device AD9361 is stored, the data of AD9361 is converted by MATLAB and make the data format is the same with the HSDC Pro data file.
when the data file loaded into the High Speed Data Converter Pro GUI tool, it was found that the waveform displayed in the Frequency Domain is inconsistent with the spectrum we have drawn using MATLAB. And the AD9361 data transmitted from the DAC3484 is not monitored by the Agilent spectrum analyzer.
I would like to ask: In the data loaded process, whether the data format has been changed in the High Speed Data Converter Pro GUI. If it has not changed, please help us analyze the reason. The figure below shows the performance of the AD9361 data in MATLAB and High Speed Data Converter Pro GUI.
Ps: AD9361 data sampling rate is 61.44MSPS, signal bandwidth is 15MHz
Question 2:
We use the tools in the TSW1400 Pattern Generators to generate LTE data sampling rate of 61.44MHz and bandwidth of 10MHz TM1.1 data.
I would like to ask: Why is the spectrogram obtained when doing FFT in MATLAB and the spectrum displayed in TSW1400 Pattern Generators inconsistent?
The figure below shows the spectrum performance in the TSW1400 Pattern Generators and the spectral representation of the data in the MATLAB spectrum.
Looking forward to reply,thank you!