Dear sir/madam,
For my current design i opted for the ADS1292R to be able to measure resp. and ECG. We are using the 2 electrodes setup and that works perfect. We have made a filter setup for safety and for filtering. Now this is working perfect but after adding a big current consuming switching device also to the test setup i am starting to see the on/off switching current peaks (of that device) in my respiratory signal. Adding a capacitor of appr. 68nF to the output of the RLD amplifier to GND (because this amplifier is used to get 1/2Vdd) and this cleared this problem in stationary situation. But when the other divice is driven harder (meaning higher turn on currents) the switching peakes can again be seen on the RR signal.
These peaks on the RR signal are very high and short peaks and could easily be fitlered in software, but i could also get a better capacitive buffering on the RLD amplifier output part of the ADS1292R. But i want to make shure that i'm not loading the RLD ampl to mutch with capacitive load. what would be the safe maximum capacitive load for this internal amplifier?
Greetings,
Laurent