This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ADS7947: what's the current capacity of internal ESD diode?

Intellectual 1520 points

Replies: 3

Views: 93

Part Number: ADS7947

Hi 

customer want to know what's the current capacity of internal ESD diode?

thanks.

  • Hi Max,

    In general, 10mA is the maximum sustained current for any current source/sink with the ADS7947. Please do let us know if you need any additional detail.

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    hi tom,

    thank you for your feedback, 10mA was the source / sink current of ADS7947.
    but the our question was about the internal ESD diode of each analog input.
    when use the internal ESD diode as clamp diode, what's the current capacity that the diode can handle?

    tony
  • In reply to tony Yao:

    The absolute maximum current is 10mA but we typically recommend keeping the current to <1mA if the diodes are expected to conduct regularly.

    Regards,
    Collin Wells
    Precision ADC Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.