THE FPGA can't configure the output pin level to the CML, then how to understand the cml level?? The FPGA GTH pin how to connect with the DAC RX[0:7] interface?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
THE FPGA can't configure the output pin level to the CML, then how to understand the cml level?? The FPGA GTH pin how to connect with the DAC RX[0:7] interface?
William,
The FPGA must be able to support the physical layer of the JESD204B standard if it is to work with the JESD204B DAC38RF82. What FPGA are you trying to use? If the transceivers support the standard, it will work with this part.
Regards,
Jim
William,
Under the DAC38RF82EVM product folder on the TI website you can download an example firmware project that is used with a Xilinx KCU105 evaluation board to interface to a DAC38RF82EVM. You find other examples as well on the Xilinx website.
Regards,
Jim