Do you have an overview for the Bio-Potential ADC portfolio available?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sure do!
The table below provides an overview of our Bio-Potential family of devices. All of the devices shown below are highly-integrated delta-sigma ADCs which incorporate many common signal chain blocks found in bio-potential applications (i.e. ECG, EEG, EMG, etc.) and integrates them into one package.
Additionally, links to the product page, datasheet, and EVM (Evaluation Module, if available) for each of the devices are shown below:
ADS1191: Datasheet, ADS1192: Datasheet, EVM
ADS1194: Datasheet, ADS1196: Datasheet, ADS1198: Datasheet, EVM
ADS1291: Datasheet, ADS1292/2R: Datasheet, EVM
ADS1294/4R: Datasheet, ADS1296/6R: Datasheet, ADS1298/8R: Datasheet, EVM/R EVM
ADS1299-4: Datasheet, ADS1299-6: Datasheet, ADS1299: Datasheet, EVM