This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ADS1261EVM: Register map is not visible and device can not be switched back from firmware update

Prodigy 20 points

Replies: 2

Views: 210

Part Number: ADS1261EVM

Hi,

I purchased ADS1261EVM to test some application. I have installed Delta-Sigma ADC EvaluaTIon Software software and drivers and when I started software I saw that board is connected but the register map on startup screen was not visible. I tried several things but the register map was still not visible. Then I started to play with buttons and of course, I put it to firmware update mode so now I can't do anything. I noticed a post on this forum that has a description of how to solve that. I followed those steps but when I got to a part where I had to locate FIRMWARE_UPDATE.bat this file was not at a specified location.

I would like to ask if this file can be posted somehow so we can download it, or if it can be added to installation package again? Then I would like to ask if there is some specific procedure to be able to see a register map when a device is connected or this should be automatically detected.

Thank you very much for your help

Matej

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.