ADS5295 evm and TSW1400 evm - problems using an external 50MHz sampling clock
Dear TI ADC team,
I am using the ADS5295 evm and TSW1400 evm and the associated ADS5295_96 GUI and HSDC Pro control software.
When using the on board oscillator operating at 80MHz, I get "clean" 12bit data on all eight channels - no dropouts in the time data, and a "clean" FFT at the carrier (testing at 3.111MHz and 30.111MHz).
When I use an external oscillator operating at 80MHz and 1.8Vp-p using the transformer input outlined in Diagram 3 on pages 31 and 32 of the ADS5295 Users Manual (SLAU442 Nov 2012), I also get
clean" data captures.
However, when I use a 50MHz sampling clock (again at 1.8Vpp), I get "noisy" data, especially on channel 1; the FFT has an increased noise floor, and one can clearly see drop outs in the time data sequence.
I am wondering if I need to change LVDS settings in the ADS5295 GUI software when I change the external sampling clock frequency.
I need to figure this out so I can use the ADS5295 with an alternative FPGA and processor in another design, so I appreciate any guidance.
Thanks!