hi
i use ads1248 to measure 3 wire PT1000, i can measure a correct value when connecting a high precision resistance.
but it has a problem when i detect if a sensor exist or not, using burnout current. sometimes it give me a wrong information .
below is register i set:
MUX0 = 0xC8 (burnout is 10uA, AIN1 is positive input, AIN0 is negative input)
VBIAS = 0x00
MUX1 = 0x30 (internal reference is on)
SYS0 = 0x22
IDAC0 = 0x90 (turn off)
IDAC1 = 0xFF(turn off)
as datasheet said:"In case of an open circuit in the sensor, these burn-out current sources pull the positive input towards AVDD and the negative input towards AVSS, "
does that mean , positive input will have a voltage ,equal to AVDD? negative input have a voltage , equal to AVSS.
in this design , AVDD = 3.3V ,AVSS = GND.
after setup register , i halt the software, using a multimeter to measure voltage on AIN1 and AIN0 , no voltage on that,
confused!!!