Other Parts Discussed in Thread: ADS54J66
Hi Team,
I have taped out an IC with 2 output pins: an output clock signal at 208.333MHz and an output analog signal. I intend to use the ADS54J66 EVM to process the signals and use my IC clock output as the external ADC sampling clock. I have read the post below and the attachment from Jim ADS54J66_500M_Ext_CLK.pptx is very helpful.
But I have 3 more questions
1. My clock signal is 0-1.2V is that ok?
2. My clock signal is 208.3333MHz instead of 500M. Are my software setup same as was recorded in the ppt?
3. My labmate warned me about the potential damage due to removing caps and re-solder them back and forth. Are there any recommendations? Or if I break the caps, can I ask what are their values?
Thank you so much!