This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1675REF: the maximum number of samples one can get from ADS1675REF using the ADCPro

Part Number: ADS1675REF

Hi guys. The user guide says ADS1675REF can capture and save 8M 24-bit sampled ADC data in the SDRAM per single acquisition. Can I use the EVM Plug-In of the ADCPro software to record and save all the 8M data to an excel or text file? It says the maximum block size for any test is 1M samples per channel. Does it mean the maximum number of samples the ADCPro software can get from the ADC1675REF for one acquisition is only 1M? 

Thanks!