Hi,
I'm using the ADS1293 EVM board, however with an external Teensy 3.6 and not the on board Microcontroller (as the ADS1293 is only one part of another, larger project). Using the register config for a 3 channel ECG and attached ECG simulator I can get nice output data (stream reading the data loop register), until all of a sudden the DRDYB signals stop coming. I've confirmed this with an oscilloscope, screenshots attached (I hope they uploaded correctly). I'm not doing anything in the code that should stop the device and I'm pretty sure it was working in an earlier test. I can still see very small spikes on the DRDYB pin in the same frequency as the Interrupt signals were coming in earlier. The durations for which I do get the interrupt singnals are random. I have confirmed that nothing is wrong with the evaluation board in general (using the ADS1293EVM test software).
I can not see anything relevant in the error registers once the data stops coming (or before for that matter, as I'm also interrupting on the Alarm pin):
ERROR_LOD: 0x00
ERROR_STATUS: 0x00
ERROR_RANGE1: 0x00
ERROR_RANGE2: 0x00
ERROR_RANGE3: 0x00
ERROR_SYNC: 0x00
ERROR_MISC: 0x00
If anyone has an idea that could help? For now, I'll read out all other registers to see if anything is amiss there...
Thank you!