Part Number: TSW14J56EVM
Hello,
I use TSW40RF832EVM board plug with TSW14J56revD board. I set boards with TSW40RF8x EVM and HSDC pro. In HSDC pro I use firmware ADC32RF80_LMF_841 and DAC38RF8x_LMF_841, like this i have expected result.
Now I would like customize FPGA, for that I use TSW14J56RevD Respin Fw.qar. I don't modify the Quartus project and I don't have same result as before. I try to modify paramater of jesd_top_qsys module in Quatus according to ADC32RF80_LMF_841.ini and result are always wrong.
For loading the FPGA I proceed like this :
1- Load FPGA with Quartus
2- I clic on button "reset DAC Jesd Core & SYSREF TRIGGER" in TSW40RF8x EVM software
3- Load pattern in HSDC pro DAC section
4- I select DAC38RF8x_LMF_841.ini file, I clic on "send" button without load firmware
5- In ADC section, i select ADC32RF80_LMF_841.ini and clic on "capture" button without load firmware
Why i don't have same result when i load the FPGA with Quartus?
regards,
Damien LUPO