HI,
With somes electromagnetics perturbations the DAC81416EVM fall in shut-down mode and when I read the status register (0x02) bit 0 (TEMP-ALM) and bit 3 (RESERVED ???) are set to "1".
What does mean the bit 3?
Why an error temperature when the Vtempout=1,25V?
How can I reset this error? The set to "1" of ALM-RESET bit in the TRIGGER register works well for the TEMP-ALM but not for the bit 3.
Regards,
Laurent Lefevre.