Other Parts Discussed in Thread: ADS114S08, ADS114S08B, TMUX1208
Hello engineers
I'm currently working on a project for university where one task is to measure ten Pt100 in the temperature range of 0°C to 200°C. The goal is to reach a accuracy of 0.1°C, even though I think that's a little bit enthusiastic. Anyway, I created a schematic using the ADS124S08 and would like to have an opinion to check if I correctly interpreted the information available in the datasheet and the application notes/cookbooks.
I intended to cycle IDAC1 through AIN0, AIN3, AIN6 and AIN9. This way it should be possible to measure four Pt100 with one single ADS124S08, right?
The following conditions apply for the design:
- Excitation current IDAC1=1mA
- Less than 10 SPS expected
- I calculated a gain value of 8 for the PGA
- The filter calculation results are added to the schematic, see green text
- Start and reset will be performed over the serial interface
The corresponding schematic sheet is attached to this post. Any tips would be highly appreciated, especially from somebody that has used the IC before. If more information is needed from my side, let me know.
Thanks in advance,ThomasADS124S08_Schematic_Draft.pdf