This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DDC264EVM: DDC264EVM read sampled data from multiple boards

Prodigy 60 points

Replies: 6

Views: 225

Part Number: DDC264EVM

Hello,

we are developing a software to read the sampled data from 7   DDC264EVM boards (connected via USB to a PC) using the USB_IO_for_VB6.dll

We are able to read the the FPGA registers of the 7 boards using the WriteFPGARegsC function  passing to it the USB device we want to read from.

And we are able to read the sampled data using the function FastAllDataCap.

The problem is that is such function doesn't exist a parameter to pass to select the USB port to read from (in order to select the board) and we are able to read only the data of  just one of the 7 boards.

Please could you suggest us how we can select the board to read from with the FastAllDataCap function?

By the way, also uising tyor software I can't select the board to read from.

 

Thanks,

Rosario 

 

  • Hi Rosario,

    Sorry but the person that developed the DLL left the team long ago and we can't support it beyond what is documented out there. That is what we say that the DLL is delivered "as is". Maybe there is something at a higher level that you can do (some kind of USB bridge) but no idea... Other than that, let's see if anyone else can add some info here (maybe to the second part of your email) but otherwise, I don't think we know how to do what you are requesting. 

    Sorry can't be of more help,

    Eduardo

  • In reply to Eduardo Bartolome:

    Hi Rosario,

    Regarding your question on the FastAllDataCap function, your inference is correct.

    It has not been designed to take the USB dev port reference as an input parameter.

     

    Regards

    Praveen

    TI makes no warranties and assumes no liability for applications assistance or customer product design. You are fully responsible for all design decisions and engineering with regard to your products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning your designs.

  • In reply to Eduardo Bartolome:

    Hi Eduardo,

    thanks for your reply.

    Please is it possible to have the USB_IO_for_VB6.dll source code along with your DDC264 demo software code so we can try do modify the dll to add the USB port parameter in the FastAllDataCap function?

    If we'll succed, we can make the updated dll available for the community.

    Thanks,

    Rosario

  • In reply to rosario lo giudice:

    Hi Rosario,

    Sorry for late answer but I was hoping someone else would comment. I am not familiar with the details of the code (I don't even have it myself...). Let me ping some other folks...

    Regards,

    Eduardo

  • In reply to Eduardo Bartolome:

    Hi Rosario,

    Please refer to the e2e link below regarding the DLL source code.

    https://e2e.ti.com/support/data-converters/f/73/p/852231/3152663#3152663

    I will close this post.

    Regards

    Praveen

    TI makes no warranties and assumes no liability for applications assistance or customer product design. You are fully responsible for all design decisions and engineering with regard to your products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning your designs.

  • In reply to Praveen Aroul:

    Thank you very much.

    BR,

    Rosario

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.