• Resolved

TSW14J56EVM: HSDC Pro new release

Intellectual 300 points

Replies: 10

Views: 189

Part Number: TSW14J56EVM

Hello,

I was wondering if there are any news in regard with the release of HSDC Pro 5.1?

I ask this because in the current release when embedding the use of the FPGA within a C or Matlab software, the data extracted from the FPGA are saved on an array, which incredibly slows things down. I was told in the past that it should have been ready on May and then July.

It would be great if there could be an update on this.

Kind regards,

Francesco

  • Guru 55430 points

    Francesco,

    The new version should be available on-line in a week or so. You can download it from the link below.

    Regards,

    Jim

    txn.box.com/.../jotagy1ms71yntbtbxa97wjiinve8zz6

  • In reply to jim s:

    Hi,

    thanks for the quick reply and for the link. 

    Kind regards,

    Francesco

  • In reply to jim s:

    Hi Jim,

    Could you please send me a link as well please, the link you sent is invalid for me.

    kelly

  • In reply to Francesco Raffaelli:

    Hi Francesco,

    could you please share your experience with the latest HSDC Pro software? Can it directly output a vector contains samples, instead of writing first.

    best wishes,

    Kelly

  • In reply to Kelly:

    Hi Kelly,

    So for what I can see so far, there is a function in the manual that enable to output array of data instead of saving them into a file. 

    Although it is useful in itself as a function, it seems not to be faster than the previous version when the data were saved on a csv file. Not clear why this is the case, though.

    This would require clarifications from TI engineers.

    best wishes,

    Francesco

  • In reply to Francesco Raffaelli:

    Hi Francesco,

    Thank you for your reply. Would it be possible to share the new update with me via like one Drive, or Dropbox, or Box? The link Ti sent you is not valid for me. I’ve asked them to send the new update to me but seems like they just ignore my request.

    Best wishes,

    Kelly

  • In reply to Kelly:

    Hi Kelly,
    sorry, I read this think just now.
    Please try this link:
     
    Kind Regards,
    Francesco
  • In reply to Francesco Raffaelli:

    Hi Francesco,

    Thank you for sending me the link, but this is the same link Ti sent you which is invalid for me, it says the file is removed or unavailable for me. What do you see when you click the link?

    Best wishes,

    Kelly

  • Guru 55430 points

    In reply to Kelly:

    Kelly,

    Please try this link.

    Regards,

    Jim

    txn.box.com/.../9laf8her9ogwmcoejln51i0w1x9vstr5

  • In reply to jim s:

    Thanks Jim. I'll give it a try and get back to you if I have any problems.

    Kelly