I've the same kind of problem. I use stm32f302r8 microcontroller (nucleo-f302r8) and adc1256. I don't receive any data through my spi communication. I've shared my code. Kindly help me through this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I've the same kind of problem. I use stm32f302r8 microcontroller (nucleo-f302r8) and adc1256. I don't receive any data through my spi communication. I've shared my code. Kindly help me through this.
Hi Gokul,
Welcome to the TI E2E Forums!
Are you able to read and write from any of the ADS1256 device registers or is the main issue your facing have to do with programming the SPI peripheral on the STM MCU?
Unfortunately, I am not familiar with that MCU and won't be able to help with code that is specifically related to the microcontroller; However, if you have the SPI peripheral working and sending commands to the ADS1256, I certainly can comment on the interfacing code for the communication to the ADC.
Have you tried probing the SPI signals on an oscilloscope or logic analyzer to verify if any of the HAL_GPIO_WritePin() or HAL_SPI_Transmit() commands are working as expected?
Feel free to share any of those screenshots with me and I'll see if I can help your debug the issue with the SPI communication.
FYI: The code you shared appears to have been truncated...I did not see the end of the adc_read() function. Feel free to share the rest of the code and I'll look it over to see if I can spot any issues.
Dear Hall,
My spi peripheral is working properly and I only have problems in sending and receiving the bytes on the adc. I just dont know where the problem is. I.ve shared the code and kindly verify
/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * <h2><center>© Copyright (c) 2019 STMicroelectronics. * All rights reserved.</center></h2> * * This software component is licensed by ST under BSD 3-Clause license, * the "License"; You may not use this file except in compliance with the * License. You may obtain a copy of the License at: * opensource.org/licenses/BSD-3-Clause * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ uint8_t receive[2]; /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ SPI_HandleTypeDef hspi3; UART_HandleTypeDef huart2; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_SPI3_Init(void); static void MX_USART2_UART_Init(void); /* USER CODE BEGIN PFP */ void adc_write(uint8_t address, uint8_t value) { uint8_t data[3]; data[0] = 0x50|address; data[1] = 0x00; data[2] = value; HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_RESET); HAL_SPI_Transmit(&hspi3, data,3, 50); //DWT_Delay(10); HAL_Delay(1); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_SET); } void adc_write_command(uint8_t command) { HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_RESET); HAL_SPI_Transmit(&hspi3,&command,1,50); HAL_Delay(1); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_SET); } /* float freq(float volta) { int value= 0, tim_val[100]; float frequency; for(int i=0;i<100;i++) { if(volta<0.1 && volta>0) { //start timer while(!(volta<0.1 && volta>0)); //stop timer } //tim_val[i] = timercount_value; value += tim_val[i]; } value = value/100; value = value*2; frequency = 1/value; return frequency; } */ int adc_read() { uint8_t datacon; uint32_t convert = 0x00; HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_RESET); adc_write_command(0x01); //read for(int i=0;i<3;i++) { HAL_SPI_Receive(&hspi3,&datacon,1,50); convert |= datacon; convert<<=8; } //DWT_Delay(10); HAL_Delay(1); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_SET); return convert; } float volt(uint32_t data2) { float v; v =(float) data2*0.000000596046; // 8388607 = +5.000v reference voltage return v; } void adc_read_regis(uint8_t address1) { uint8_t data1[3]; data1[0] = 0x10|address1; data1[1] = 0x00; HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_RESET); HAL_SPI_Transmit(&hspi3, data1, 2, 50); HAL_Delay(5); HAL_SPI_Receive(&hspi3,&data1[2],1,50); //DWT_Delay(10); HAL_Delay(1); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_SET); } void adc_reset() { HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_RESET); HAL_GPIO_WritePin(GPIOC, RESET_Pin, GPIO_PIN_RESET); HAL_Delay(1); HAL_GPIO_WritePin(GPIOC, RESET_Pin, GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_SET); } void adc_init() { adc_write(0x00, 0x03); //status adc_write(0x02, 0x20); //adcon adc_write(0x03, 0x82); //drate 100sps adc_read_regis(0x03); //verification adc_write_command(0xF0); //selfcab of adc adc_write(0x01, 0x0F); //mux for channel 0 positive adc_write_command(0xFC); //sync adc_write_command(0x00); //wake up HAL_Delay(500); } /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ uint32_t adc_data_ch0, adc_data_ch1; float voltage_ch0, voltage_ch1; /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_SPI3_Init(); MX_USART2_UART_Init(); /* USER CODE BEGIN 2 */ MX_GPIO_Init(); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_RESET); adc_reset(); HAL_Delay(500); MX_SPI3_Init(); HAL_Delay(500); adc_write_command(0xFE); //reset to power up values adc_write_command(0xFC); //sync adc_write_command(0x00); //wake up //DWT_Delay(10); HAL_Delay(1); adc_init(); HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET); //confirm configuration MX_USART2_UART_Init(); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_RESET); //while(HAL_GPIO_ReadPin(DRDY_GPIO_Port,DRDY_Pin)); adc_write(0x01, 0x1F); //mux for ch1 positive channel adc_write_command(0xFC); //sync adc_write_command(0x00); //wake up adc_data_ch0 = adc_read(); voltage_ch0 = volt(adc_data_ch0); //while(HAL_GPIO_ReadPin(DRDY_GPIO_Port,DRDY_Pin)); adc_write(0x01, 0x0F); //mux for ch0 positive channel adc_write_command(0xFC); //sync adc_write_command(0x00); //wake up adc_data_ch1 = adc_read(); voltage_ch1 = volt(adc_data_ch1); //frequency_in_ch1 = freq(voltage_in_ch1); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { HAL_Delay(100); HAL_Delay(100); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_SET); } /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Initializes the CPU, AHB and APB busses clocks */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL8; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB busses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) { Error_Handler(); } } /** * @brief SPI3 Initialization Function * @param None * @retval None */ static void MX_SPI3_Init(void) { /* USER CODE BEGIN SPI3_Init 0 */ /* USER CODE END SPI3_Init 0 */ /* USER CODE BEGIN SPI3_Init 1 */ /* USER CODE END SPI3_Init 1 */ /* SPI3 parameter configuration*/ hspi3.Instance = SPI3; hspi3.Init.Mode = SPI_MODE_MASTER; hspi3.Init.Direction = SPI_DIRECTION_2LINES; hspi3.Init.DataSize = SPI_DATASIZE_8BIT; hspi3.Init.CLKPolarity = SPI_POLARITY_LOW; hspi3.Init.CLKPhase = SPI_PHASE_1EDGE; hspi3.Init.NSS = SPI_NSS_SOFT; hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16; hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi3.Init.TIMode = SPI_TIMODE_DISABLE; hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi3.Init.CRCPolynomial = 7; hspi3.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi3.Init.NSSPMode = SPI_NSS_PULSE_ENABLE; if (HAL_SPI_Init(&hspi3) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI3_Init 2 */ /* USER CODE END SPI3_Init 2 */ } /** * @brief USART2 Initialization Function * @param None * @retval None */ static void MX_USART2_UART_Init(void) { /* USER CODE BEGIN USART2_Init 0 */ /* USER CODE END USART2_Init 0 */ /* USER CODE BEGIN USART2_Init 1 */ /* USER CODE END USART2_Init 1 */ huart2.Instance = USART2; huart2.Init.BaudRate = 38400; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART2_Init 2 */ /* USER CODE END USART2_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOC, RESET_Pin|CHIP_SELECT_Pin, GPIO_PIN_SET); /*Configure GPIO pin : B1_Pin */ GPIO_InitStruct.Pin = B1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : LD2_Pin */ GPIO_InitStruct.Pin = LD2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : DRDY_Pin */ GPIO_InitStruct.Pin = DRDY_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(DRDY_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : RESET_Pin CHIP_SELECT_Pin */ GPIO_InitStruct.Pin = RESET_Pin|CHIP_SELECT_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(char *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
Hi Gokul,
See my comments in the code snippet below:
int adc_read() { uint8_t datacon; uint32_t convert = 0x00; // TODO: Consider making this a signed 32-bit value, since the ADC data is signed HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_RESET); // TODO: Insert a short delay here (between /CS low and first SCLK), // unless HAL_GPIO_WritePin() already provide sufficent delay to meet the ADS1256's "t3" timing requirement. adc_write_command(0x01); // TODO: Don't set /CS high after sending this byte! // TODO: Insert a short delay here to meet the "t6" timing requirement // NOTE: Some MCUs use FIFOs to store the MISO data from the SPI peripheral. Make sure that this FIFO has been cleared // before calling HAL_SPI_Receive(), or else the DONT CARE return byte from the previous "0x01" command may be mis-interpreted as data. for(int i=0;i<3;i++) { // TODO: Send a "0x00 byte" to clock out the ADC data byte, unless HAL_SPI_Receive() already does this... HAL_SPI_Receive(&hspi3,&datacon,1,50); convert |= datacon; convert<<=8; } // TODO: Consider appending sign-extension byte to "convert" (based on most-significant bit of ADC data), see the following URL for an example: // https://e2e.ti.com/blogs_/archives/b/precisionhub/archive/2016/04/01/it-s-in-the-math-how-to-convert-adc-code-to-a-voltage-part-1 HAL_Delay(1); HAL_GPIO_WritePin(GPIOC, CHIP_SELECT_Pin, GPIO_PIN_SET); return convert; }
I hope that helps!
Dear hall,
@christopher hall rest of code looks fine? I mean I got to change the convert data type to signed datatype and introduce a short delay after sending rdata command. Will sending a 1ms delay work?. And I'll also work on the fifo miso output. Is it ok to reset the chip select at the initial code and phase and never set till the end. Other parts of adc_init() looks ok? Kindly point out all other errors possible because I'm not sure whether data is getting written on the status or adcon or drate registers. When I try to read back the data I get a big fat zero. You can see my read reg code. Kindly help me with the same .
Hi Gokul,
Assuming your using the nominal 7.68 MHz clock for the ADS1256, then the "t6" delay only needs to be about 6 us. The datasheet says "t3" can be a minimum of 0 ns, but I would recommend making it at least 50 ns.
If you make these delays too long then it will take you longer to clock out the ADC data, and this could present a problem when trying to run the ADC at the faster data rates.
/CS is used to selected which device on the SPI bus you want to talk to, so if you only have one device on the SPI bus, then technically you can leave it low. However, I would strongly advise against using /CS in this way...
/CS prevents the slave device from responding to SCLKs while it is high. Therefore, to protect the MCU and ADC from getting out of sync (due to noise or glitches on the SCLK signal), only set /CS low to issue a command (or read data) and then set it back high when your done. Each time you set /CS low, the ADC's SPI peripheral is reset to look for the beginning of the next command and this helps keep the SPI communication in alignment between the master and slave.
I looked through additional parts of your code and had the following comments
Dear Hall,
Christopher Hall (1528318) Hi! All your points were really helpful and I did implement in my program. Unfortunately still I don't receive the conversion data. I'll share you two codes one with arduino and another with stm32f302r8. The code works perfectly in arduino i.e displaying two conversion data from two channels(ain0 and ain1 both positive channel) in the serial monitor. But when I try to do the same with stm32f302r8 it doesn't work. I've initialized my spi in spi mode 1 (i.e) CPHA 2 edge and COPL LOW. I've uploaded the oscilloscope image of clk, miso and mosi signal in both arduino for your reference. in case of stm32f302r I dont see any signal in my miso pin. Can you please help me in debugging my problem since I'm fairly new to the controller world. Kindly comment on the waveforms in both arduino and stm32f302r8 board because I really doubt with drdy signal. Thanks for the replies earlier! Sorry for the long post.waveform.rar
Arduino code
/* ADS1256 CLK - pin 13 DIN - pin 11 (MOSI) DOUT - pin 12 (MISO) CS - pin 10 DRDY - pin 9 RESET- pin 8 (or tie HIGH?) DVDD - 3V3 DGND - GND */ #define cs 10 // chip select #define rdy 9 // data ready, input #define rst 8 // reset pin #define pwd 7 // power down #define flag 0 // #define SPISPEED 1000000 // 1250000 #define rdata 0x01 #include <SPI.h> //byte data = 0b00000000; void mux( byte data) { SPI.transfer(0x50 | 1); // MUX register SPI.transfer(0x00); // 2nd command byte, write one register only SPI.transfer(data); // write the databyte to the register delayMicroseconds(10); } void sync() { //SYNC command 1111 1100 SPI.transfer(0xFC); delayMicroseconds(10); //WAKEUP 0000 0000 SPI.transfer(0x00); delayMicroseconds(10); } void calculation() { int32_t adc_val =0; float V = 0; adc_val = SPI.transfer(0); adc_val <<= 8; //shift to left adc_val |= SPI.transfer(0); adc_val <<= 8; adc_val |= SPI.transfer(0); V = adc_val*0.000000596046; // 8388607 = +5.000v / delayMicroseconds(10); Serial.println(adc_val, HEX); Serial.print("+"); Serial.println(V); } void setup() { Serial.begin(115200); int8_t data; pinMode(cs, OUTPUT); digitalWrite(cs, LOW); // tied low is also OK. pinMode(rdy, INPUT); pinMode(rst, OUTPUT); digitalWrite(rst, LOW); delay(1); // LOW at least 4 clock cycles of onboard clock. 100 microsecons is enough digitalWrite(rst, HIGH); // now reset to deafult values //delay(500); SPI.begin(); //start the spi-bus //delay(500); //init digitalWrite(pwd, LOW); //while (digitalRead(rdy)) {} // wait for ready_line to go low SPI.beginTransaction(SPISettings(SPISPEED, MSBFIRST, SPI_MODE1)); // start SPI delayMicroseconds(10); //Reset to Power-Up Values (FEh) SPI.transfer(0xFE); delayMicroseconds(10); byte status_reg = 0 ; // address (datasheet p. 30) //PGA SETTING //1 ±5V //2 ±2.5V //4 ±1.25V //8 ±0.625V //16 ±312.5mV //32 ±156.25mV //64 ±78.125mV //byte status_data = 0x01; //status: Most Significant Bit First, Auto-Calibration Disabled, Analog Input Buffer Disabled byte status_data = 0b00000110; SPI.transfer(0x50 | status_reg); SPI.transfer(0x00); // 2nd command byte, write one register only SPI.transfer(status_data); // write the databyte to the register delayMicroseconds(10); Serial.println("status done"); SPI.transfer(0x01 | status_reg); SPI.transfer(0x00); // 2nd command byte, write one register only delayMicroseconds(25); data = SPI.transfer(0xFF); Serial.println(data, HEX); delayMicroseconds(10); byte adcon_reg = 2; //A/D Control Register (Address 02h) byte adcon_data = 0x20; // 0 01 00 000 => Clock Out Frequency = fCLKIN, Sensor Detect OFF, gain 1 SPI.transfer(0x50 | adcon_reg); SPI.transfer(0x00); // 2nd command byte, write one register only SPI.transfer(adcon_data); // write the databyte to the register delayMicroseconds(10); Serial.println("adcon done"); // Set sampling rate byte drate_reg = 3; byte drate_data = 0b11110000; // 100SPS SPI.transfer(0x50 | drate_reg); SPI.transfer(0x00); SPI.transfer(drate_data); delayMicroseconds(10); Serial.println("drate done"); SPI.transfer(0xF0); delay(500); // digitalWrite(cs, HIGH); Serial.println("configured, starting"); mux(0b00001111);//DIFF 1 sync(); delay(500); } void loop() { Serial.println(); //Serial.println("adc"); // digitalWrite(cs, LOW); SPI.beginTransaction(SPISettings(SPISPEED, MSBFIRST, SPI_MODE1)); // start SPI delayMicroseconds(10); while (digitalRead(rdy)== 1) {} ; mux(0b00011111);//DIFF 1 sync(); Serial.println("pot"); SPI.transfer(rdata); // Read Data 0000 0001 (01h) delayMicroseconds(10); calculation(); delayMicroseconds(10); // digitalWrite(cs, HIGH); //SPI.endTransaction(); /* //The ADS1255/6 output 24 bits of data in Binary Two's //Complement format. The LSB has a weight of //2VREF/(PGA(223 − 1)). A positive full-scale input produces //an output code of 7FFFFFh and the negative full-scale //input produces an output code of 800000h. if(adc_val > 0x7fffff){ //if MSB == 1 adc_val = (16777215ul - adc_val) + 1; //do 2's complement Serial.print("-"); } else { Serial.print("+"); } */ //mV /= 1000; delay(100); Serial.println(); while (digitalRead(rdy)== 1) {} ; mux(0b00001111); sync(); //SYNC command 1111 1100 SPI.transfer(0xFC); delayMicroseconds(10); //WAKEUP 0000 0000 SPI.transfer(0x00); delayMicroseconds(10); Serial.println("ldr"); SPI.transfer(rdata); // Read Data 0000 0001 (01h) delayMicroseconds(10); // digitalWrite(cs, HIGH); //SPI.endTransaction(); calculation(); }
Stm32f302r8 code
#include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ UART_HandleTypeDef hlpuart1; UART_HandleTypeDef huart3; SPI_HandleTypeDef hspi1; TIM_HandleTypeDef htim6; PCD_HandleTypeDef hpcd_USB_OTG_FS; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_LPUART1_UART_Init(void); static void MX_USART3_UART_Init(void); static void MX_TIM6_Init(void); static void MX_USB_OTG_FS_PCD_Init(void); static void MX_SPI1_Init(void); /* USER CODE BEGIN PFP */ void delay() //create delay of 26us { __HAL_TIM_ENABLE(&htim6); while(__HAL_TIM_GET_FLAG(&htim6, TIM_FLAG_UPDATE)==0); __HAL_TIM_DISABLE(&htim6); __HAL_TIM_CLEAR_FLAG(&htim6, TIM_FLAG_UPDATE); } void adc_write(uint8_t address, uint8_t value) { uint8_t data[3]; data[0] = 0x50|address; data[1] = 0x00; data[2] = value; delay(); HAL_SPI_Transmit(&hspi1, data,3, 10); delay(); } void adc_write_command(uint8_t command) { delay(); HAL_SPI_Transmit(&hspi1,&command,1,10); delay(); } int adc_read() { uint8_t datacon; int32_t convert = 0x00; delay(); adc_write_command(0x01); //read delay(); for(int i=0;i<3;i++) { HAL_SPI_TransmitReceive(&hspi1,0xFF,&datacon,1,10); convert |= datacon; convert<<=8; } return convert; } void adc_reset() { HAL_GPIO_WritePin(GPIOB, RESET_Pin, GPIO_PIN_RESET); HAL_Delay(1); HAL_GPIO_WritePin(GPIOB, RESET_Pin, GPIO_PIN_SET); } void adc_init() { delay(); adc_write_command(0xFE); delay(); adc_write_command(0x0F); delay(); adc_write(0x00, 0x02); //status delay(); adc_write(0x02, 0x20); //adcon delay(); adc_write(0x03, 0x82); //drate 100sps delay(); adc_write_command(0xF0); //selfcab of adc delay(); HAL_Delay(100); //100ms delay } /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ int32_t adc_data_ch0, adc_data_ch1; /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_LPUART1_UART_Init(); MX_USART3_UART_Init(); MX_TIM6_Init(); MX_USB_OTG_FS_PCD_Init(); MX_SPI1_Init(); /* USER CODE BEGIN 2 */ HAL_GPIO_WritePin(GPIOB, CHIP_SELECT_Pin, GPIO_PIN_RESET); adc_reset(); MX_SPI1_Init(); HAL_GPIO_WritePin(GPIOB, PDWN_Pin, GPIO_PIN_RESET); adc_init(); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { HAL_GPIO_WritePin(GPIOB, CHIP_SELECT_Pin, GPIO_PIN_RESET); delay(); adc_write(0x01, 0x0F); //mux for channel 0 positive delay(); adc_write_command(0xFC); //sync delay(); adc_write_command(0x00); //wake up delay(); while(HAL_GPIO_ReadPin(DRDY_GPIO_Port,DRDY_Pin)); adc_data_ch1 = adc_read(); HAL_GPIO_WritePin(GPIOB, CHIP_SELECT_Pin, GPIO_PIN_SET); HAL_Delay(100); HAL_GPIO_WritePin(GPIOB, CHIP_SELECT_Pin, GPIO_PIN_RESET); delay(); adc_write(0x01, 0x1F); //mux for channel 0 positive delay(); adc_write_command(0xFC); //sync delay(); adc_write_command(0x00); //wake up delay(); while(HAL_GPIO_ReadPin(DRDY_GPIO_Port,DRDY_Pin)); adc_data_ch0 = adc_read(); HAL_GPIO_WritePin(GPIOB, CHIP_SELECT_Pin, GPIO_PIN_SET); HAL_Delay(100); HAL_GPIO_WritePin(GPIOB, LD2_Pin,1); delay(); HAL_GPIO_WritePin(GPIOB, LD2_Pin,0); delay(); /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_PeriphCLKInitTypeDef PeriphClkInit = {0}; /** Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB busses clocks */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 8; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB busses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) { Error_Handler(); } PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_LPUART1 |RCC_PERIPHCLK_USB; PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1; PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1; PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_PLLSAI1; PeriphClkInit.PLLSAI1.PLLSAI1Source = RCC_PLLSOURCE_HSE; PeriphClkInit.PLLSAI1.PLLSAI1M = 1; PeriphClkInit.PLLSAI1.PLLSAI1N = 12; PeriphClkInit.PLLSAI1.PLLSAI1P = RCC_PLLP_DIV2; PeriphClkInit.PLLSAI1.PLLSAI1Q = RCC_PLLQ_DIV2; PeriphClkInit.PLLSAI1.PLLSAI1R = RCC_PLLR_DIV2; PeriphClkInit.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_48M2CLK; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) { Error_Handler(); } } /** * @brief LPUART1 Initialization Function * @param None * @retval None */ static void MX_LPUART1_UART_Init(void) { /* USER CODE BEGIN LPUART1_Init 0 */ /* USER CODE END LPUART1_Init 0 */ /* USER CODE BEGIN LPUART1_Init 1 */ /* USER CODE END LPUART1_Init 1 */ hlpuart1.Instance = LPUART1; hlpuart1.Init.BaudRate = 209700; hlpuart1.Init.WordLength = UART_WORDLENGTH_7B; hlpuart1.Init.StopBits = UART_STOPBITS_1; hlpuart1.Init.Parity = UART_PARITY_NONE; hlpuart1.Init.Mode = UART_MODE_TX_RX; hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1; hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; hlpuart1.FifoMode = UART_FIFOMODE_DISABLE; if (HAL_UART_Init(&hlpuart1) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN LPUART1_Init 2 */ /* USER CODE END LPUART1_Init 2 */ } /** * @brief USART3 Initialization Function * @param None * @retval None */ static void MX_USART3_UART_Init(void) { /* USER CODE BEGIN USART3_Init 0 */ /* USER CODE END USART3_Init 0 */ /* USER CODE BEGIN USART3_Init 1 */ /* USER CODE END USART3_Init 1 */ huart3.Instance = USART3; huart3.Init.BaudRate = 115200; huart3.Init.WordLength = UART_WORDLENGTH_8B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_NONE; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16; huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart3) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART3_Init 2 */ /* USER CODE END USART3_Init 2 */ } /** * @brief SPI1 Initialization Function * @param None * @retval None */ static void MX_SPI1_Init(void) { /* USER CODE BEGIN SPI1_Init 0 */ /* USER CODE END SPI1_Init 0 */ /* USER CODE BEGIN SPI1_Init 1 */ /* USER CODE END SPI1_Init 1 */ /* SPI1 parameter configuration*/ hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_2EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 7; hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE; if (HAL_SPI_Init(&hspi1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI1_Init 2 */ /* USER CODE END SPI1_Init 2 */ } /** * @brief TIM6 Initialization Function * @param None * @retval None */ static void MX_TIM6_Init(void) { /* USER CODE BEGIN TIM6_Init 0 */ /* USER CODE END TIM6_Init 0 */ TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER CODE BEGIN TIM6_Init 1 */ /* USER CODE END TIM6_Init 1 */ htim6.Instance = TIM6; htim6.Init.Prescaler = 0; htim6.Init.CounterMode = TIM_COUNTERMODE_UP; htim6.Init.Period = 31; htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim6) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM6_Init 2 */ /* USER CODE END TIM6_Init 2 */ } /** * @brief USB_OTG_FS Initialization Function * @param None * @retval None */ static void MX_USB_OTG_FS_PCD_Init(void) { /* USER CODE BEGIN USB_OTG_FS_Init 0 */ /* USER CODE END USB_OTG_FS_Init 0 */ /* USER CODE BEGIN USB_OTG_FS_Init 1 */ /* USER CODE END USB_OTG_FS_Init 1 */ hpcd_USB_OTG_FS.Instance = USB_OTG_FS; hpcd_USB_OTG_FS.Init.dev_endpoints = 6; hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED; hpcd_USB_OTG_FS.Init.Sof_enable = ENABLE; hpcd_USB_OTG_FS.Init.low_power_enable = DISABLE; hpcd_USB_OTG_FS.Init.lpm_enable = DISABLE; hpcd_USB_OTG_FS.Init.battery_charging_enable = ENABLE; hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE; hpcd_USB_OTG_FS.Init.vbus_sensing_enable = ENABLE; if (HAL_PCD_Init(&hpcd_USB_OTG_FS) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USB_OTG_FS_Init 2 */ /* USER CODE END USB_OTG_FS_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); HAL_PWREx_EnableVddIO2(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, CHIP_SELECT_Pin|RESET_Pin|PDWN_Pin, GPIO_PIN_SET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, LD3_Pin|LD2_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : B1_Pin */ GPIO_InitStruct.Pin = B1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : DRDY_Pin */ GPIO_InitStruct.Pin = DRDY_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_PULLUP; HAL_GPIO_Init(DRDY_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : CHIP_SELECT_Pin RESET_Pin PDWN_Pin */ GPIO_InitStruct.Pin = CHIP_SELECT_Pin|RESET_Pin|PDWN_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pins : LD3_Pin LD2_Pin */ GPIO_InitStruct.Pin = LD3_Pin|LD2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pin : USB_PowerSwitchOn_Pin */ GPIO_InitStruct.Pin = USB_PowerSwitchOn_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(USB_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : USB_OverCurrent_Pin */ GPIO_InitStruct.Pin = USB_OverCurrent_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USB_OverCurrent_GPIO_Port, &GPIO_InitStruct); } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(char *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
Hi Gokul,
I would recommend probing the /DRDY signal on the ADS1256 first to ensure that it is active. You should see a periodic waveform, with the time between /DRDY falling edge corresponding to the data rate. If you don't then you'll need to check that the ADC is properly powered, the GPIO configured correctly, and that the device is clocked.
How are you connecting the ADS1256 to the STM MCU? Do you have a common ground between these devices?
On one of your waveforms (with the Arduino) it looked like DOUT did not have a stable ground reference voltage.
NOTE: When probing the SPI signals, make sure to probe them near the ADC, and ground the oscilloscope to the ADC's ground potential so that you can see what the ADC sees.
Dear Hall,
I checked all the things you mentioned and I still unable to get the converted data from adc to the stm32f302r8 board. I kindly request you to go through both codes and try to point the errors in my stm32f302r8 code. I've shared the code in the previous comment. I think I'm missing out some thing in my code. Please help me in finding out the missing part in my code. fyi the arduino code which i shared in the previous comment works perfectly. My spi clock geerates 1Mhz clock with clock polarity low and clock phase 2 edged. Kindly help me with the same.
Hi Gokul,
Would it be possible for you to capture some more oscilloscope screenshots of the SPI communication? (Ideally showing the /CS, DIN, DOUT, SCLK signals).
I looked through you code once and didn't see any obvious errors. If you're still running into issues then I think look at the SPI signals will be the easiest way to troubleshot.
Dear Hall,
I dont get any waveform in my Dout pin. I really dont know what is the problem. I've shared you the Din and Sclk waveform and I've enabled a gpio pin for chip select which is made low all the time. I'm also getting a periodic signal in my DRDY pin. Is there any chance that the data's may not be written in the status adcon and drate registers. If my SPI is not working then I would never get a Din waveform, but in my case I'm getting it. I think the conversion is not happening in the adc side and moreover is there any 8-bit data transfer register in the adc side. If not from where are we fetching the converted data. Please correct me if I'm wrong. Thank you once again for speedy replies.
Hi Gokul,
How is the ADS1256 connected to your STM MCU? Are you jumping wiring to the ADS1256EVM, or have you built your own PCB?
If you're seeing a periodic /DRDY signal, but no DOUT while senidng SCLKs, then either the ground reference between the MCU and ADC is floating, or maybe /CS is being held high.
Dear Hall,
Christopher Hall I'm using waveshare high resolution ADC and Nucleo- F302R8 MCU board. I'm using jumping wires to connect both the boards. Today I checked my code and found out that DRDY pin is always high and got stuck at this statement "while(HAL_GPIO_ReadPin(DRDY_GPIO_Port,DRDY_Pin))" . I've also verified that they are connected to the common ground. What could be the problem?
Dear Hall,
Christopher Hall As I said earlier, I'm trying to interface waveshare adc with nucleo -f302r8 board. Right now I'm able to convert the data and receive it in my micro controller but I'm facing a different set of problem. The received data is not within the scale limit. I've given my reference voltage as 2.5V and my register value as follows.
Status register = 0x02
ADCON = 0x20
Drate = 0x82
input mux = 0x0F aincom = grnd //postive channel
when i give a 0v in ain0 I'm getting 800000 as output and for 5V I'm getting BFFFFF
0V - 800000 5V - BFFFFF
input mux = 0xF0 aincom = grnd //negative channel
when i give a 0v in ain0 I'm getting FFFFFF as output and for 5V I'm getting C00000
0V - 800000 5V - C00000
Moreover my data is kinda oscillating and give any suggestion to keep it steady.
Hi Gokul,
What are you using for you input signal source and how is it connected and biased with respect to the ADS1256? If you have a schematic of your circuit that you could share it would be very helpful.
It seems as if your input signal source is connected to a difference ground reference than the ADS1256. You may also want to probe your reference voltage to ensure that it is stable. If the reference voltage is oscillating then you may get unexpected and oscillating ADC output codes.
Best regards,
Chris
Dear Hall,
Christopher Hall Thank you so much for your help. It seems that ground was the problem from the initial stage. Now the conversion is happening and I'm able to read a more precise value up to 5 decimal points. Even though the conversion is happening i find some mismatch in samples per second values. So, I read all the three registers (status, adcon and drate) after writing with some values leaving a sufficient delay time of 500ms. Turns out that the values doesn't match. Please look at the data below. Can you please assist me with this problem. But even with this mismatch I'm getting the correct conversion data. schematic link(https://www.waveshare.com/w/upload/2/29/High-Precision-AD-DA-board.pdf) for your reference).
Registers | Written value(HEX) | Read value after 500ms(HEX) |
Status | 0x06 | 0x30 |
Adcon | 0x20 | 0x20 |
Drate | 0x82 | 0xF0 |
Dear Hall,
Christopher Hall As I mentioned earlier my adc working fine, but i have problems writing in the register yet still I'm able to get the converted data. Please check my previous comment. I got 2 questions to be addressed. Kindly help me with the same.
Question 1: The values which I'm writing in the status, adcon, drate registers doesn't match with the values which I read after 100ms in the same registers.
But the values which I write in the MUX register matches and I've verified it by varying dynamically. Kindly help me with the problem.
Question 2: The drate value defaults to 0xF0(since drate value is not updating when I write on it) which is 30ksps and I've verified that value with my drdy signal in an oscilloscope.
The problem is when I give an input as sinusoidal signal of frequency 1Hz(time period = 1sec) I get only 2.8k samples for a sec.
My assumption is that if I set as 30ksps then for a sine wave with time period of 1sec should get 30k samples, but when I read the samples I get only 2.8k samples. I've set my spi clock frequency is 2MHz. Please correct me if I wrong.
What should I do to achieve at least a minimum of 10k samples ?
Hi Gokul,
As this question is somewhat a duplicate to your other post, see my responses here:
https://e2e.ti.com/support/data-converters/f/73/p/859187/3177623#3177623
Best regards,
Bob B