Hi Team,
ADS7953 datasheet tells that if full-scale input span is set to Range 2, 2xVref should be no higher than +VA, may I know what will be the output if 2xVREF > +VA?
For example, Vref is 2.5V, +VA is 5V provided by the LDO, the LDO output cannot be always be 5V due to the accuracy error, what will it be if the LDO output changes to 4.95V?
Thanks and Best Regards!
Hao