Other Parts Discussed in Thread: AFE5809,
Hi, everyone!
I am developing an application, which controls AFE5809 chip via SPI.
For testing I am using development board “AFE5809 EVM REV.A”. I connect to it via connector P14 (it is placed on board). SPI chip ouputs are connected to P14 on board.
But at the moment I cannot even switch chip to test pattern generation mode. In the same time, when I use software from development board kit, the SPI chip works well in all modes.
I can see that during connect the software sends some starting sequence of commands to the chip. I think I miss something when I try to initialize SPI chip from my application.
Could you write an example of initializing sequence for AFE5809 (which registers I should write and what sequence exactly), so I could switch the chip into mode for generating test pattern?
Thanks very much.