Dear all
We have an application where we have 5 ADS1248 connected to various sensors.
We ave 5 different CS, one common ADSTART and one common RESET, they are connected in parallell on the SPI-Bus
On each AD we have 2 RTDs connected and we are using the internal IDACs for excitating the sensors, current set for 1mA.
Now we are experiencing spurious "resets" on them, sometimes all of them, and sometimes some of them, as it seems that the IDAC0 and IDAC1 registers is overwritten, it also happens that only one of the IDACS is shut down, leaving the other IDAC operating normally.
Since they share the same HW-RESET, it cannot be a hardware reset, since all of them would have been reset simultainiously.
We have been searching both source-code and assembler output for any hint on what is happening, sofar we ended upp in nothing that coukd explain why they are selectivly reset.
Is there any condition in the actual chip that could cause an internal reset, like overloading IDACs etc (now, I cannot understand how to overload a current generator), or anything else that could cause this behaviour.