Other Parts Discussed in Thread: ADS1292
Hi,
I'm currently working with the ADS1292R. I can read and write any register but I'm unable to read conversion data in either RDATAC or RDATA mode (DRDY pin doesn't seems to work).
I'm using the internal clock oscillator, the internal reference buffer is enabled and set at 2.42V. The oversampling rate is set to 500SPS and both channels input are set to input short (as suggest in figure 63 of the datasheet).
I followed figure 63 procedure from the datasheet but DRDY never toggle. If I try to get the output without starting a conversion, I don't even receive the correct status bits (0xC00).
By probing with an oscilloscope, I can see DVDD = 3.2V, AVDD = 3.2V, VCAP1 = 1.52V but VCAP2 = 0V and Vrefp = 0V.
I would think that the device might be broken since VCAP2 and Vrefp = 0, but since the spi communication still works, I'm not sure what is going on?
I'm I missing any step in the device setup?
Thanks a lot!
Jacob.