Hi Joseph,
I also interested in the input leakage current. But that current is caused by the protection diodes (shown in Figure 8 in datasheet) instead of the capacitors! I have already found a typical value in sbaa355 application note:
"Based on the typical characteristics curves, the absolute input current is 250nA depending upon temperature, input voltage, and input channel."
We want to use this ADC in our new product that will working in wide temperature range (-40°C..+85°C) with relative large resistors on the inputs. On large resistors the input bias current could be caused significant error, so this parameter is important. Could you provide a more specific characteristic about the bias current? It would be very helpful for us.
Thank you for your help in advance!
Peter