Other Parts Discussed in Thread: ADS131E08, , OPA330
Hi, I have hardware that reads straing gauges powered by 3.3V, uses an ADS131E08 with PGA = 12 and VREF = 2.4V.
I am reading voltages between (1.65V + 0.2V) to (0.2V - 1.65V) with full 24 bits resolution.
Range: 1.85V to 1.45V (referenced to 1.65V).
I am planning to change the A / D converter to ADS131M08, as it is smaller and cheaper.
The strain gauges will be powered with 3V on the new hardware, so they will generate a voltage referenced to 1.5V.
My idea was to amplify the strain gauge signal to vary between (1.5V + 1.2V to 1.5V - 1.2V) and use all 24-bit resolution when PGA = 1.
The new input voltage range must be: 2.7V to 0.3V (referenced to 1.5V)
However after reading some questions on the forum, I was unsure if I could use it in the same way.
From what I understand in the forum topics, I could use it only to read voltages between 1.2V to -1.2V referenced to AGND (0V).
Range: 1.2V to -1.2V (reference to AGND (0V) )
So if I were to use ADS131M08 with single supply I would need to condition the signal to vary between 0V and 1.2V and the resolution would be only 23bits.
I would like to understand this better, the datasheet does not make it clear.