This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TLV320AIC3204EVM-K: unable to set up digital loopback on the EVM

Part Number: TLV320AIC3204EVM-K

I am attempting to set up an audio IP on IP1 and send it to line out via the digital loopback path. If I use the analog capability to do the same thing, everything is OK. It appears the problem is in the ADC/DAC, perhaps clock setup. I have tried everything I can think of using the GUI.I have been carefully through the clock setup and believe I have it set correctly. Because of internal dependencies on the order of doing things, do I need to run a script? Does anyone have a script to do this on the EVM they are willing to share. Any help is much appreciated.

Many thanks, Ron

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.