To implement interactive voice response system, my application required to read data from the dataflash and convert that into audio signal using DAC.
Can anybody provide app note/source code for intergacing TLV320DAC32 with MSP430 microcontroller?
Please give suggestion for below things :
1. I have .wav audio file, in which format data has to be stored in data flash?
2. Please mention clock settings of TLV320DAC32.
3. Is there any GUI to configure internal registers of TLV320DAC32.
Advance Thanks.
Hello,
I am looking for sample source code for TLV320DAC32.
I am interfacing TLV320DAC32 with LPC1768 controller.
Kindly share code, if anybody done.
Thanks
here is an app note for interfacing the AIC26 to the MSP430. You will find that the DAC32 is very similar to the DAC on the AIC26 so this same info should be useful.
http://www.ti.com/lit/an/slaa449a/slaa449a.pdf