we are using DM37XX/AM37xx evm KIT.
we are using TLV320AIC3254 codec ( I2C + MCBSP2 Interface) on linux version 2.6.32 ( Android2.3) FOR OMAP3EVM.
when we are trying to play music from Android Music Players it shows following logs :
I/TIALSAModule( 983): Initialized ALSA PLAYBACK device defaultI/ActivityManager( 940): Displayed activity com.android.music/.MediaPlaybackActivity: 463 ms (total 463 ms)E/AudioHardwareALSA( 983): RE-OPEN AFTER STANDBY:: took 608 msecsW/AudioFlinger( 983): write blocked for 609 msecs, 7 delayed writes, thread 0x4bf08W/AudioTrack( 983): obtainBuffer timed out (is the CPU pegged?) 0x58808 user=00002800, server=00000800W/AudioTrack( 983): obtainBuffer timed out (is the CPU pegged?) 0x58808 user=00002800, server=00000800W/AudioTrack( 983): obtainBuffer timed out (is the CPU pegged?) 0x58808 user=00002800, server=00000800W/AudioTrack( 983): obtainBuffer timed out (is the CPU pegged?) 0x58808 user=00002800, server=00000800
can u plz help us ?