Hello,
My customer is starting to implement the following path using the EVM
But seems to be stuck in this mode, since he can't seem to hear any of the effects take place
Can someone please provide the settings for the EVM software that he should be using.
Thanks
Looks like one of the pictures was not inserted, the path my customer is looking for IS
To enable the effects filters on the record path the following must be done:
1. ensure that the DAC's are powered down in R37
2. program the effect filter coefficients
3. enable ADC processing in R107
4. enable effects filter in R12