I am using a TLV320AIC3254EVM-K and have generated Pure Path Process Flows and the corresponding script files. I have had good success loading script files with the AIC3254CS application using the "Command-Line Interface".
Could someone please direct me to a (simple) command line application (or source code) that can be used to write I2C script files to the AIC3254 via the TAS1020 (on a TLV320AIC3254EVM-K) in lieu of using either of the TI Pure Path Studio or AIC3254CS applications.
Thank You,
Brian Weir
Hi, Brian,
Let me move this to the Audio Converters e2e where the converter guys hang.
-d2
-----
Don Dapkus
Audio Applications Engineering Manager
Dallas, TX USA
Hi Brian,
We don't have source code we can provide to communicate between to the TAS1020B from the PC as it is for internal use only.
Is there anything in particular you wanted to do that we can help you with?
Regards,
J-
Jorge,
Does the TAS1020B application translate incoming HID reports into I2C commands? If so, I've got a sample windows app that might serve as a starting-point.
Frank