Hi,
I use PurePath 1.88 buid 5 with a TAS3204 since 2 years. Now, i created a "big" file with 24 Volume faders, some mixers and so on. I compiled and saved the file with no issues yesterday. Today, when I tried to open the project, it gives me a message to close the purepath studio yes, no, abort. When i click to abort, all connections are lost and some (2-5) componens are also lost.
In the output window is written (german installation):
Der Objektverweis wurde nicht auf eine Objektinstanz festgelegt.
Is the file to big for the purepath studio? I tried it a second time and also this version was corrupt.
I want to make a mixer unit with 6 inputs and 4 outputs, and with the "normal" mixer unit, i have no fade-in and fade-out characteristics, thats why i used the 6x4 volume faders.
Please tell me, if this amount of components is not recommended.
thanks, Michael