The PCM2906 minimum specified temperature range is -25°C, while the absolute minimum ambient temperature rating under bias is -40°C. If an application requires regular operation down to -40°C, what are the major repercussions to performance? It is suspected the part will function fine at -40°C, other than that the DAC and ADC accuracies will be out of spec (which is of no concern for this application). Could you please comment on whether the -40°C tolerance of this part will suffice, or if an alternative solution is available?