I have been using the TLV320AIC3254 quite successfully for a while now. However, in Bypass Mode (and probably all mode) I have noticed that the device stops working and goes into what I assume is power down (<1mA) after about 10 minutes. I have reduced the audio levels both internally (via the registers and externally) to next to nothing without success.
IO_Vdd = 1.8v or 3V3
AVdd = 1.8V
DVdd = 1.8V
lDO_IN = O/C
The total current consumption of the device (when working normally) = 7.62mA.
I have tried all sorts of PSU configuration with out change.
Re-programming the registers resets the device.
Any help would be appreciated.